AXIS#.SAFEPARAM.SLP_#.POSLOWERLIMIT

Description

Indicates the absolute position lower limit of the Safely Limited Position (SLP) safety function.

 

Parameters Editor with the Position Lower Limit (s_LL_SLP) circled

 

This is s_LL_SLP in the following diagram:

 

Context

For complete SLP information refer to SLP (Safely Limited Position).

Related safety parameters:

Versions

Action Version Notes

Implemented

02-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

Depends on user units

Range

[-2^31+1, 2^31-1]

Default Value

1

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SLP_1.POSLOWERLIMIT

316ch

05h

Signed32

-

-

Read/Write

No

AXIS1.SAFEPARAM.SLP_2.POSLOWERLIMIT

316dh

05h

Signed32

-

-

Read/Write

No

AXIS1.SAFEPARAM.SLP_3.POSLOWERLIMIT

316eh

05h

Signed32

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLP_1.POSLOWERLIMIT

326ch

05h

Signed32

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLP_2.POSLOWERLIMIT

326dh

05h

Signed32

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLP_3.POSLOWERLIMIT

326eh

05h

Signed32

-

-

Read/Write

No